Hi community,
I have a question about MMPF0100.
MMPF0100 has FUSE_PORx bits , however there is no description about these bits in MMPF0100 datasheet (Rev.7.0).
Could you let me know the function of these bits?
Best Regards,
Satoshi Shimoda
解決済! 解決策の投稿を見る。
OTP fuse bit FUSE_POR can be blown so that upon subsequent power cycles, the start-up sequence
is chosen from the OTP fuses and not from the TBBOTP registers.
Hi Yuri,
Thank you for your reply.
Then, I want t to know the difference between FUSE_POR1, FUSE_POR2, and FUSE_POR3 also.
I guess the start-up sequence is defined as below.
If this is correct, there is no difference between FUSE_POR1, FUSE_POR2, and FUSE_POR3.
Is this right?
Best Regards,
Satoshi Shimoda
Correct, any of the FUSE_PORx may be used, no difference between them.