FTM_CNT value changing in quadrature encoder mode without any movement at the encoder end. Can somebody help intialize FTM in quadrature encoder mode with output compare match?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTM_CNT value changing in quadrature encoder mode without any movement at the encoder end. Can somebody help intialize FTM in quadrature encoder mode with output compare match?

761件の閲覧回数
tan_k
Contributor II

I am currently using colibri imx 7 som. I am trying to initialize the quadrature encoder mode with ouput compare match. The code given below the intialization of registers as per the instructions given in the manual. I do see change in the FTM count register even though the enoder is not moving. Are there any other changes I need to make to the FTM registers or any other registers in conjuntion to make the code functional

//initialization is mentioned on pg 4197

FTM_FMS=0x00000000; //6 WPEN 0 Write Protection Enable

FTM_MODE |=(1<<FTMEN); 

FTM_SC &= ~((1<<CLKS_0)|(1<<CLKS_1)); 

FTM_CONF |=(1<<BDMMODE_1)|(1<<BDMMODE_0);


FTM_POL=0x00000003;

FTM_OUTMASK =0x0000007A; 


FTM_QDCTRL &= ~((1<<QUADMODE)|(1<<QUADEN));

FTM_CNTIN=0x00000000;

FTM_C7SC=0x0000001C; 

FTM_COMBINE=0x00000000;

FTM_C7V=0x00006000; 


FTM_DEADTIME=0x00000000; 

FTM_FILTER=0x00000044;

// FTM_INVCTRL=0x00000000; //not used


//FTM_SWOCTRL=0x00000000; //not used

// FTM_OUTINIT=0x00000000; //not used


FTM_SC |=(1<<CLKS_0); 

FTM_QDCTRL |=(1<<PHBFLTREN)|(1<<PHAFLTREN)|(1<<QUADEN);


FTM_MODE &=~(1<<FTMEN);


FTM_SYNCONF |= (1<<SYNCMODE)|(1<<SWRSTCNT)|(1<<SWWRBUF)|(1<<SWOM); 


FTM_SYNC |= (1<<SWSYNC) |(1<<CNTMAX)|(1<<SYNCHOM) ;

FTM_CNT=0x00000000; //0-15 COUNT 0x000 Counter Value

ラベル(1)
0 件の賞賛
返信
0 返答(返信)