FSL Ubuntu 0912 Sources

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FSL Ubuntu 0912 Sources

1,352件の閲覧回数
Davros
Contributor III

Greetings Everyone,

When we received the iMX51 Babbage prototype board, there was an SD card with ubuntu on it, specifically the sticker on the back of the SD card mentions "FSL UBUNTU 0912".

I am trying to duplicate what is on the SD card, so I downloaded  the L2.6.31_09.12.01_SDK_source.  In its configuration there is an option for "FSL gnome release package", however nothing mentioned ubuntu.  

Please let me know what I need to download, or change in order to build this.

Many thanks,

Daryl W. Jarman

タグ(1)
0 件の賞賛
返信
1 返信

1,281件の閲覧回数
KursadOney
NXP Employee
NXP Employee

Hi Daryl,

My understanding is the Ubuntu SDK comes from Linaro. The linaro-linux-mx51 launchpad page might be a good place to start looking.

0 件の賞賛
返信