FSL_MIRROR imx8mq error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FSL_MIRROR imx8mq error

2,322件の閲覧回数
haihoang
Contributor II

Hi,

I'm building yocto imx4.14.98-2.0.0-ga for imx8mq-evk board.

I see that the downloads directory contains some .bin file: firmware-imx-8.1.bin, firmware-qca-2.0.3.bin, ...

According to i.MX_Linux_Release_Notes.pdf, page 4, these files can be retrieved using the following command on the Linux OS: wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/*file.bin*

Unfortunately, this command is failed.

And, I look at the bitbake file, these .bin files are fetched from FSL_MIRROR: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/ . Again, this link is died.

So, please let me know the alternative link, or where to fetch these .bin files.

タグ(2)
0 件の賞賛
返信
1 返信

2,259件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I can download the bin files.

Maybe the network is not very stable recently. Please try it again.

0 件の賞賛
返信