FRDM-MX95 AAOS 16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-MX95 AAOS 16

970 Views
FlynHawaiian
Contributor I

Will Android AAOS 16 image from nxp install on the FRDM-MX95?

 

Secondarily, can an m.2 hard drive be installed in the slot?

0 Kudos
Reply
3 Replies

899 Views
FlynHawaiian
Contributor I

1) Is it possible I can build an android 16 image, as you say the source code for the frdm is there.  

2) Is there a particular reason that AAOS 16 couldn't be run on the FRDM-MX95?  Since the processor is a MIMX9596XVTXNAC, it has full features and the only difference is the memory speed.  The MX95EVK uses the MIMX9596AVZXNAC.  

Since both processors are full function processors I can't imagine there being a reason that AAOS nor Android shouldn't be able to be installed on the FRDM-mx95 board.  Could you shed some light on the reasoning?

0 Kudos
Reply

694 Views
saajid
Contributor I
Hello Flyn,

I am also looking for an Android image or source package compatible with the FRDM-i.MX95. Have you found anything suitable?
0 Kudos
Reply

910 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

NXP documentation supports Android 16 and AAOS on i.MX 95 EVK/Verdin boards—not FRDM-IMX95, for the Android 16 BSP have the source code for the FRDM-95, but we have not rest it by now. And the FRDM-IMX95 does include an M.2 Key-M slot intended for AI cards and SSDs.

0 Kudos
Reply