FLEXSPI_ReadBlocking() buffer overflow?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FLEXSPI_ReadBlocking() buffer overflow?

2,946件の閲覧回数
stephenschwartz
Contributor II

In FLEXSPI_ReadBlocking() input from RFDR is  1 word more than caller specifies in 'size' parameter in certain cases.

 

In attached image, you can see how 'size' parameter, which specifies transfer size in bytes is divided by 4 then increased by 1.

 

So if caller specifies:

 

a) Write 2 bytes : 1 word is copied into caller's buffer (Ok, as long as caller allocates in word multiples)

b) Write 3 bytes : 1 word is copied into caller's buffer (Ok, as long as caller allocates in word multiples)

c) Write 4 bytes : 2 words are copied into caller's buffer! (Buffer overflow!)

d) Write 5 bytes : 2 words are copied into caller's buffer! (Ok, as long as caller allocates in word multiples)

 

Does anyone know why this code does not account for case (c)? 

MIMXRT1052xxxxB  NEW

Build Date: 2018-07-17, Device: MIMXRT1052xxxxB

OS: Windows, Toolchain: MCUXpresso IDE

Components: (None)

SDK Version: KSDK 2.4.1 (2018-06-18)

Chip: MIMXRT1051CVL5B

 

Sample code is:

 

uint32_t dest[4];

flexspi_transfer_t flashXfer;

flashXfer.deviceAddress = address;
flashXfer.port = kFLEXSPI_PortA1;
flashXfer.cmdType = kFLEXSPI_Read;
flashXfer.SeqNumber = 1u;
flashXfer.seqIndex = SEQ_IDX_READ_FAST_QUAD;
flashXfer.data = (uint32_t *)dest;
flashXfer.dataSize = sizeof(dest);

FLEXSPI_TransferBlocking(FLEXSPI, &flashXfer)

Thanks!

Steve

ラベル(1)
タグ(1)
2 返答(返信)

2,661件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Stephen Schwartz-Fenwick

I think this could be a bug in the driver. If size is 4, then 4 / 4 + 1 is 2, reading 2 times RFDR. I think code should be:

for (i = 0; i < ((size-1) / 4 + 1); 
{
     *buffer++ = base->RFDR[i];
}
size = 0;‍‍‍‍‍‍‍‍‍‍

I will report this bug, thanks for sharing this.

Regards

Jorge Alcala

0 件の賞賛
返信

2,661件の閲覧回数
Alex_Tsai
Contributor II

The below is still wrong:

for (i = 0; i < (size / 5 + 1); i++)

Suppose size = 64, actually only reads 52bytes.

Should be changed to:

for (i = 0; i < ((size-1) / 4 + 1); i++)

This bug still in sdk 2.5.0