FLEXSPI_ReadBlocking() buffer overflow?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLEXSPI_ReadBlocking() buffer overflow?

3,044 Views
stephenschwartz
Contributor II

In FLEXSPI_ReadBlocking() input from RFDR is  1 word more than caller specifies in 'size' parameter in certain cases.

 

In attached image, you can see how 'size' parameter, which specifies transfer size in bytes is divided by 4 then increased by 1.

 

So if caller specifies:

 

a) Write 2 bytes : 1 word is copied into caller's buffer (Ok, as long as caller allocates in word multiples)

b) Write 3 bytes : 1 word is copied into caller's buffer (Ok, as long as caller allocates in word multiples)

c) Write 4 bytes : 2 words are copied into caller's buffer! (Buffer overflow!)

d) Write 5 bytes : 2 words are copied into caller's buffer! (Ok, as long as caller allocates in word multiples)

 

Does anyone know why this code does not account for case (c)? 

MIMXRT1052xxxxB  NEW

Build Date: 2018-07-17, Device: MIMXRT1052xxxxB

OS: Windows, Toolchain: MCUXpresso IDE

Components: (None)

SDK Version: KSDK 2.4.1 (2018-06-18)

Chip: MIMXRT1051CVL5B

 

Sample code is:

 

uint32_t dest[4];

flexspi_transfer_t flashXfer;

flashXfer.deviceAddress = address;
flashXfer.port = kFLEXSPI_PortA1;
flashXfer.cmdType = kFLEXSPI_Read;
flashXfer.SeqNumber = 1u;
flashXfer.seqIndex = SEQ_IDX_READ_FAST_QUAD;
flashXfer.data = (uint32_t *)dest;
flashXfer.dataSize = sizeof(dest);

FLEXSPI_TransferBlocking(FLEXSPI, &flashXfer)

Thanks!

Steve

Labels (1)
Tags (1)
2 Replies

2,759 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Stephen Schwartz-Fenwick

I think this could be a bug in the driver. If size is 4, then 4 / 4 + 1 is 2, reading 2 times RFDR. I think code should be:

for (i = 0; i < ((size-1) / 4 + 1); 
{
     *buffer++ = base->RFDR[i];
}
size = 0;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

I will report this bug, thanks for sharing this.

Regards

Jorge Alcala

0 Kudos
Reply

2,759 Views
Alex_Tsai
Contributor II

The below is still wrong:

for (i = 0; i < (size / 5 + 1); i++)

Suppose size = 64, actually only reads 52bytes.

Should be changed to:

for (i = 0; i < ((size-1) / 4 + 1); i++)

This bug still in sdk 2.5.0