FLAC, WAV format

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FLAC, WAV format

8,649件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I want to ask about a method of realizing a high-resolution audio system with i.MX6 and Linux.

Customer wants to use 192KHz/24bit FLAC and WAV format.

I think that the FLAC is encoded data, and WAV is raw data.

It seems that the Yocto Linux includes the codec for FLAC.

 

 

Q1.

Can I understand that it is able to realize a high-resolution audio system (192KHz/24bit FLAC and WAV format) by using the i.MX6 with Yocto Linux(L4.1.15)?

 

Q2.

Can I understand that it uses the ESAI(DACDAT, LRCLK, BCLK) to send the FLAC decoded data or WAV raw data from i.MX6 to a codec device?

 

Best Regards,

 

ラベル(2)
0 件の賞賛
返信
1 返信

8,506件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

1. right.

2. correct, please refer to attached Release Notes Table 27. Parser/Demuxer supported audio/video

and Linux Manual Chapter 28 Advanced Linux Sound Architecture (ALSA) System on a Chip (ASoC)

Sound Driver sect.28.2.2 7.1 Audio Codec Features, p.224, 225

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信