imx7s booting from emmc - mmc2: error -84 initialising MMC card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx7s booting from emmc - mmc2: error -84 initialising MMC card

1,371 次查看
edwardtyrrell
Senior Contributor I

Hi All,

I have an issue booting a custom imx7s board, 90% of the time I'll get the error: Waiting for root device /dev/mmcblk1p2...
mmc2: error -84 whilst initialising MMC card. However it does seem to get to the login prompt after the initial dd of the Kernel and FS, but any time its ran after that it fails with the same error. What is error -84?

My build is fsl-community-bsp  -  krogoth ( Yocto ).

I've compared the custom board's partitioning with a development board ( warp7 ) which its based on and UMS side of things seem to match ( FAT32 0x0C and EXT4 0x83).

Thanks.

标签 (4)
0 项奖励
回复
1 回复

1,065 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Edward

emmc has partitions settings which can be programmed internally

in emmc, for example please check below hints how to make user partition read-only 

WaRP7 possible brick and solution - i.MXDev Blog 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复