FAT partition for Kernel image imx8m Mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FAT partition for Kernel image imx8m Mini

ソリューションへジャンプ
1,181件の閲覧回数
antonio_santagi
Contributor IV

Hello,

by default the Linux BSP for imx8m mini creates a FAT partition, separated from RootFS partition, that comprises the Kernel image.

What is the reason why this is a better solution than having a RootFS partition with the Kernel image in it and no FAT partition at all ?

Is it because in the case of corrupted RootFS then Kernel at least will be loaded and can try recovering the RootFS ?

 

thank you

ラベル(1)
0 件の賞賛
返信
1 解決策
1,174件の閲覧回数
b36401
NXP Employee
NXP Employee

Recently u-boot did not support ext2/ext3/ext4 filesystems and one was forced to place the kernel on FAT (or directly on the drive, outside of the filesystem).
Also you can access device tree from windows machine if you attach the card with a cardreader.

However I suppose there is no strong reason to have this FAT partition instead of using rootfs.
But it if still recommended.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,175件の閲覧回数
b36401
NXP Employee
NXP Employee

Recently u-boot did not support ext2/ext3/ext4 filesystems and one was forced to place the kernel on FAT (or directly on the drive, outside of the filesystem).
Also you can access device tree from windows machine if you attach the card with a cardreader.

However I suppose there is no strong reason to have this FAT partition instead of using rootfs.
But it if still recommended.

0 件の賞賛
返信