Hi community,
Our customer have a question about i.MX6UL pin.
Please see Table 95 in IMX6ULCEC Rev.1.
The Out of Reset Condition of many pads are "Input, value=keeper".
Our customer want to know whether external pull-up/pull-down to decide input logic, because thye think i.MX6UL will unexpected work by undifined logic if these pads are floating.
Would you let me know whether should they connect pull-up or pull-down to these pads?
Or external pull-up/pull-down is needed since internal pull-up/pull-down decide the logic?
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
Hi Satoshi
keeper prevents pad from floating, please look at
Bus-holder - Wikipedia, the free encyclopedia
if guaranteed pad input value is needed, one can use external
pull resistor, for selection overriding resistor value please check
keeper value in Table 24. Single Voltage GPIO DC Parameters i.MX6UL Datasheet
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
keeper prevents pad from floating, please look at
Bus-holder - Wikipedia, the free encyclopedia
if guaranteed pad input value is needed, one can use external
pull resistor, for selection overriding resistor value please check
keeper value in Table 24. Single Voltage GPIO DC Parameters i.MX6UL Datasheet
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
Thank you for your reply.
According to your reply, I understood external pull-up/down is not mandatory, and it is depend on a system of our customer whether external pull-up/down is needed or not.
Is this correct?
Best Regards,
Satoshi Shimoda