External clock on RGMII_TX_CTL possible for RMII?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External clock on RGMII_TX_CTL possible for RMII?

ソリューションへジャンプ
2,863件の閲覧回数
MagnusNilsson
Contributor II

I have a custom IMXDL board with a KSZ8863 switch.

According to MDIO the switch is fine, but RMII is dead silent.

Both IMXDL and PHY are clocked by external clock.

I would like to confirm that it is indeed possible to use RGMII_TX_CTL to clock RMII from an external clock?

The HW dev. guide (IMX6DQ6SDLHDG) is a bit light on detail regarding RGMII_TX_CTL, as GPIO_16 is the recommended external clock sink.

If RGMII_TX_CTL is a valid clock sink for RMII, it's a SW issue and I'd much appreciate any sample code.

I'm trying to get ethernet running on uboot, for a start.

ラベル(2)
0 件の賞賛
返信
1 解決策
2,131件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Magnus

yes this signal also can be used for RMII as described in

IMX6SDLRM Table 23-1. ENET External Signals

There are some RMII examples below

RMII on i.MX6 (L3.0.35_4.1.0)

Re: RMII interface on i.MX6 Solo

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,132件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Magnus

yes this signal also can be used for RMII as described in

IMX6SDLRM Table 23-1. ENET External Signals

There are some RMII examples below

RMII on i.MX6 (L3.0.35_4.1.0)

Re: RMII interface on i.MX6 Solo

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信