External Ref clock for PCIE Gen.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

External Ref clock for PCIE Gen.2

1,626 次查看
adiavraham
Contributor II

Hi,

The are so many topics regarding this issue, but I don't find the answer in any of them.

In IMX6, is the CLK1/CLK2 pins configured as input Ref clock for the PCIE are LVDS compatible or HCSL compatible?

Where can I find the electrical specifications of the input (common mode, dif inut swing,VIH,VIL)?

Thanks,

Adi

标签 (1)
0 项奖励
回复
2 回复数

1,445 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Adi

the LVDS interface complies with TIA/EIA 644-A standard. Please check TIA/EIA STANDARD

644-A, Electrical Characteristics of Low Voltage Differential Signaling (LVDS) Interface Circuits" for details. 

Also please look at

https://community.nxp.com/message/421885?commentID=421885#comment-421885 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,445 次查看
adiavraham
Contributor II

thanks,

Adi

0 项奖励
回复