External RTC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

External RTC

1,533 次查看
lk22
Contributor I

HI,

We are using internal RTC with a crystal of 9pF load capacitance and two 16pF capacitors on i.MX6S processor. The clock is about 2 to 3 seconds lagging behind on every 2 days. How this can be corrected?

We are thinking to use external RTC, which will provide clock on I2C lines to processor. Will there be any issue in booting or timing on using external RTC?

with regards

Lalit

标签 (2)
0 项奖励
回复
1 回复

1,396 次查看
art
NXP Employee
NXP Employee

Q. How this can be corrected?

A. Check the crystal tolerance first.

Q. Will there be any issue in booting or timing on using external RTC?

A. No, there should be no any issue. You just have to slightly modify the software to load the value of the external RTC to the internal one each boot time.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复