Example Reference IMX RT 1020 running without SDRAM MCUXpresso Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example Reference IMX RT 1020 running without SDRAM MCUXpresso Project

1,000 Views
Vliermaal
Contributor I

Morning All,

   I am looking for example / ref of 1020 running without SDRAM (MCUXpresso)

   I am on a custom 1020 without SDRAM but XIP with Segger and flashing fine

   Violates at runtime

   Modified SDK's do not provide a stable solution

Best Wishes

Don't hesitate to ask further questions

 

 

 

0 Kudos
Reply
1 Reply

985 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

One way you can try the SDK examples without using SDRAM is to reallocate the code or the compiled objects and link them to flash by modifying the linker file.

 

Regards,

Daniel.

0 Kudos
Reply