Example LPUART DMA use?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example LPUART DMA use?

2,149 Views
davenadler
Senior Contributor II

I'm using RT1024 which has nice full-function LPUARTs. I need to receive characters via DMA with a completion interrupt on either (inactivity and data received) or (received data hits high-water mark or count). In the completion ISR/callback I'll transfer the received characters (into a FreeRTOS stream buffer) and do whatever is necessary to continue DMA input processing (toggling receive buffers if this is needed).

Is there an example that shows how to do this? Can it be done using one of the FSL drivers? Please note I do not want to use a ring buffer - just give me the data please.

Thanks in advance for any help,
Best Regards, Dave

PS: Next question will be DMA output, blocking til completion (sending output lines from a queue).

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,117 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @davenadler ,

   To the RT UART DMA, please refer to our application note:

https://www.nxp.com/docs/en/application-note/AN12679.pdf

The code is:

https://www.nxp.com/docs/en/application-note-software/AN12679SW.zip

This works perfect.

 

Please check it at first.

If you still have issues about it, just kindly let me know.

Best Regards,

Kerry

0 Kudos
Reply