Ethernet interface going down when connecting to WiFi in Client Mode on imx8mplus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet interface going down when connecting to WiFi in Client Mode on imx8mplus

ソリューションへジャンプ
3,373件の閲覧回数
ssuresh
Contributor I

Hi NXP,

[Description]

When we try connecting the board to a network via client mode using wlan0 interface, once we run udhcpc command, the ethernet interface goes down.

In ifconfig, we could only see wlan0 and lo interfaces.

Please find the set of commands used:

# ifconfig wlan0 up
# cd /etc
# wpa_passphrase “ESSID” “password” > wpa_supplicant.conf
# wpa_supplicant -B -D nl80211 -i wlan0 -c wpa_supplicant.conf
# udhcpc -i wlan0

[Expected]

We need eth0, eth1 and wlan0 to be UP at the same time as per our use case.

 

[NOTE] This issue is not observed in WiFi AP Mode.

 

Please find the complete dmesg logs for reference.

0 件の賞賛
返信
1 解決策
2 返答(返信)
3,326件の閲覧回数
ssuresh
Contributor I

Hi NXP Team,

connmanctl resolved this issue.

0 件の賞賛
返信
3,361件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信