Ethernet interface going down when connecting to WiFi in Client Mode on imx8mplus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Ethernet interface going down when connecting to WiFi in Client Mode on imx8mplus

跳至解决方案
3,415 次查看
ssuresh
Contributor I

Hi NXP,

[Description]

When we try connecting the board to a network via client mode using wlan0 interface, once we run udhcpc command, the ethernet interface goes down.

In ifconfig, we could only see wlan0 and lo interfaces.

Please find the set of commands used:

# ifconfig wlan0 up
# cd /etc
# wpa_passphrase “ESSID” “password” > wpa_supplicant.conf
# wpa_supplicant -B -D nl80211 -i wlan0 -c wpa_supplicant.conf
# udhcpc -i wlan0

[Expected]

We need eth0, eth1 and wlan0 to be UP at the same time as per our use case.

 

[NOTE] This issue is not observed in WiFi AP Mode.

 

Please find the complete dmesg logs for reference.

0 项奖励
回复
1 解答
2 回复数
3,368 次查看
ssuresh
Contributor I

Hi NXP Team,

connmanctl resolved this issue.

0 项奖励
回复
3,403 次查看
jimmychan
NXP TechSupport
NXP TechSupport
0 项奖励
回复