Ethernet in External SDRAM Help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet in External SDRAM Help

5,970件の閲覧回数
kamal1
Contributor III

Hello,

I am working on a project which involves using the Ethernet in external SDRAM. I am using Keilv5 Pro edition with a custom board based off the MIMXRT1050 demo board. 

I used the Keil network demo project to test the Ethernet in QSPI flash and it works fine. When I try to use the Ethernet in SDRAM, it does not work. It appears that the Ethernet is not being initialized correctly. The Keil network configuration involves using RTOS2. I need all the project code to be stored and executed in external SDRAM. 

I am having the same issue on the MIMXRT1050 demo board in which the network Ethernet works when run through QSPI flash but when I try the same thing in external RAM, it does not work. I believe it has to do with the RTOS memory being used or memory speed differences between the QSPI flash and SDRAM. 

Is there something that needs to be set up or changed when using the Ethernet in external SDRAM? 

Best,

Kamal

0 件の賞賛
返信
7 返答(返信)

5,837件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

Sorry I don't have knowledge about RTOS RTX5 .

Please also compare the options for the Target

pastedImage_1.png

Regards

Daniel

0 件の賞賛
返信

5,837件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Kamal:

If you are using external SDRAM as your main RAM, for LwIP I would suggest you put some key data structures to SRAM_DTC or other non-cacheable region.

pastedImage_1.png

ENET buffers need to store in SRAM_DTC

Original definition:(enet_ethernetif_kinetis.c)

    SDK_ALIGN(static rx_buffer_t rxDataBuff_0[ENET_RXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

    SDK_ALIGN(static tx_buffer_t txDataBuff_0[ENET_TXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

 

Change to:

  AT_NONCACHEABLE_SECTION_ALIGN(static rx_buffer_t rxDataBuff_0[ENET_RXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

  AT_NONCACHEABLE_SECTION_ALIGN(static tx_buffer_t txDataBuff_0[ENET_TXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

I hope this helps.

Regards

Daniel

0 件の賞賛
返信

5,837件の閲覧回数
kamal1
Contributor III

Hi Daniel,

Thanks for your helpful information. I am currently using Keilv5 IDE to write code but I did go into MCUXpresso to look at what you were talking about. I don't think that is my issue. I believe the SDRAM is running too fast which is causing errors with hardware. How can I adjust the SDRAM to run at the same speed as the QSPI Flash?

I have code to run a stepper motor from Flash. When I moved the same code to SDRAM, the stepper only worked correctly when I added a 500 nanosecond delay in between steps. I feel the same issue may be occurring with the Ethernet, in which the Ethernet is not being initialized correctly due to the SDRAM clock speed.

I know the code is working at the current Flash speed so if I configure the SDRAM to run at the same speed, I believe it may solve my issues. Is the correct way to change the SDRAM main clock speed done when initializing the SDRAM from Flash or can adjusting the SDRAM clock be completed in SDRAM code? 

Is there any example of Ethernet running in external SDRAM or can one be created and sent to me?

Best,

Kamal

0 件の賞賛
返信

5,837件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

In your link file, you should have a non cacheable region to hold the buffers.
The non-cacheable region can be in SDRAM, or in SRAM_DTC.

There is a demo with LWIP in SDRAM.
Please refer to
SDK_2.7.0_EVKB-IMXRT1050\boards\evkbimxrt1050\lwip_examples\lwip_httpscli_mbedTLS\freertos\mdk

I hope it helps.
Regards
Daniel
0 件の賞賛
返信

5,827件の閲覧回数
nxf40536
NXP Employee
NXP Employee

Hi @danielchen,

I am having a similar problem while trying to run LWIP from SDRAM. I do have a noncacaheable section in the linker:

MEMORY
{
/* Define each memory region */
BOARD_FLASH (rx) : ORIGIN = 0x60000000, LENGTH = 0x800000 /* 8M bytes (alias Flash) */
SRAM_DTC (rwx) : ORIGIN = 0x20000000, LENGTH = 0x20000 /* 128K bytes (alias RAM) */
SRAM_ITC (rwx) : ORIGIN = 0x0, LENGTH = 0x20000 /* 128K bytes (alias RAM2) */
SRAM_OC (rwx) : ORIGIN = 0x20200000, LENGTH = 0xc0000 /* 768K bytes (alias RAM3) */
BOARD_SDRAM (rwx) : ORIGIN = 0x80000000, LENGTH = 0x1000000 /* 16M bytes (alias RAM4) */
NCACHE_REGION (rwx) : ORIGIN = 0x81000000, LENGTH = 0x1000000 /* 12M bytes (alias RAM5) */
}

I've replaced the above-mentioned lines in the enet_ethernetif_kinetis.c file :

 

err_t ethernetif0_init(struct netif *netif)
{
static struct ethernetif ethernetif_0;
AT_NONCACHEABLE_SECTION_ALIGN(static enet_rx_bd_struct_t rxBuffDescrip_0[ENET_RXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);
AT_NONCACHEABLE_SECTION_ALIGN(static enet_tx_bd_struct_t txBuffDescrip_0[ENET_TXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);
AT_NONCACHEABLE_SECTION_ALIGN(static rx_buffer_t rxDataBuff_0[ENET_RXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);
AT_NONCACHEABLE_SECTION_ALIGN(static tx_buffer_t txDataBuff_0[ENET_TXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

ethernetif_0.RxBuffDescrip = &(rxBuffDescrip_0[0]);
ethernetif_0.TxBuffDescrip = &(txBuffDescrip_0[0]);
ethernetif_0.RxDataBuff = &(rxDataBuff_0[0]);
ethernetif_0.TxDataBuff = &(txDataBuff_0[0]);

return ethernetif_init(netif, &ethernetif_0, 0U, (ethernetif_config_t *)netif->state);
}

I don't seem to get a hold of what's happening but there I am not receiving anything on the eth interface. 

/* DATA section for NCACHE_REGION */

.data_RAM5 : ALIGN(4)
{
FILL(0xff)
PROVIDE(__start_data_RAM5 = .) ;
PROVIDE(__start_data_NCACHE_REGION = .) ;
*(.ramfunc.$RAM5)
*(.ramfunc.$NCACHE_REGION)
*(NonCacheable.init)
*(.data.$RAM5)
*(.data.$NCACHE_REGION)
*(.data.$RAM5.*)
*(.data.$NCACHE_REGION.*)
. = ALIGN(4) ;
PROVIDE(__end_data_RAM5 = .) ;
PROVIDE(__end_data_NCACHE_REGION = .) ;
} > NCACHE_REGION AT>BOARD_FLASH

 

/* BSS section for NCACHE_REGION */
.bss_RAM5 : ALIGN(4)
{
PROVIDE(__start_bss_RAM5 = .) ;
PROVIDE(__start_bss_NCACHE_REGION = .) ;
*(NonCacheable)
*(.bss.$RAM5)
*(.bss.$NCACHE_REGION)
*(.bss.$RAM5.*)
*(.bss.$NCACHE_REGION.*)
. = ALIGN (. != 0 ? 4 : 1) ; /* avoid empty segment */
PROVIDE(__end_bss_RAM5 = .) ;
PROVIDE(__end_bss_NCACHE_REGION = .) ;
} > NCACHE_REGION AT> NCACHE_REGION

Can you please help me with this ?

Thank you,

Vlad Dascau

0 件の賞賛
返信

5,837件の閲覧回数
kamal1
Contributor III

Hello,

I have looked at the example you recommended and it does work in SDRAM. The problem is my code uses Keil RTX5 RTOS and the working example uses FreeRTOS. I have tried to adjust my code to work with FreeRTOS but I cannot get it to work. I need to use the Keil RTOS RTX5 to be able to access the SMTP functions. 

Also, I do not have these lines of code in my Keil RTX5 project:

    SDK_ALIGN(static rx_buffer_t rxDataBuff_0[ENET_RXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

    SDK_ALIGN(static tx_buffer_t txDataBuff_0[ENET_TXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

Change to:

  AT_NONCACHEABLE_SECTION_ALIGN(static rx_buffer_t rxDataBuff_0[ENET_RXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

  AT_NONCACHEABLE_SECTION_ALIGN(static tx_buffer_t txDataBuff_0[ENET_TXBD_NUM], FSL_ENET_BUFF_ALIGNMENT);

After adjusting my code while keeping Keil RTX5, I created the scatter file that almost matches the working project. In the .map file screenshots, you can see the left side is my non working project and the right side is working. I moved the network files to DTC memory just like the working project. For some reason I am missing the .bss files? 

The working project runs in Flash and the scatter files are similar. Do you know how to fix the issue with the missing .bss files?

Best,

Kamalnxp1.JPGnxp2.JPG

0 件の賞賛
返信

2,883件の閲覧回数
djr-spectrummfg
Contributor I

I found that the noncachable buffer fix proposed above did not work for my imxrt1060 project, but what did work is setting  `FSL_SDK_ENABLE_DRIVER_CACHE_CONTROL=1` for the project.

0 件の賞賛
返信