Ethernet eDMA Driver for IMIXRT1170

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet eDMA Driver for IMIXRT1170

ソリューションへジャンプ
1,905件の閲覧回数
nishantraaz
Contributor I

Hi All,

We want to use eDMA for ethernet in our project in IMIXRT1170. Is there any driver for ethernet eDMA for this Processor. If no, then how to use eDMA for ethernet.

We saw eDMA driver for various peripherals like LPUART, FlexIO etc. but this is not available for ethernet. Is there any specific reason behind that.

Tools Used:

IDE: MCUxpresso v11.4.1

SDK 2.10.1

ラベル(3)
0 件の賞賛
返信
1 解決策
1,898件の閲覧回数
Yuri
NXP Employee
NXP Employee

@nishantraaz 
Hello,

   i.MX RT1170 ENET has own unified DMA (uDMA), internal to the ENET module, which
optimizes data transfer between the ENET core and the SoC, and supports an enhanced
buffer descriptor programming model to support IEEE 1588 functionality.

  There is no need for eDMA.

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,899件の閲覧回数
Yuri
NXP Employee
NXP Employee

@nishantraaz 
Hello,

   i.MX RT1170 ENET has own unified DMA (uDMA), internal to the ENET module, which
optimizes data transfer between the ENET core and the SoC, and supports an enhanced
buffer descriptor programming model to support IEEE 1588 functionality.

  There is no need for eDMA.

Regards,
Yuri.

0 件の賞賛
返信