Errors with ltib when trying to include QT embedded

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Errors with ltib when trying to include QT embedded

1,393件の閲覧回数
blsousan
Contributor III

So I am trying to add QT embedded to my root file system using ltib.  With the other packages I simply select them, run ltib, and no problems (it adds them to the rootfs).  However, when I tried the QT embedded it had errors in finding the package at the www.bitshrine.org.  (qt-everywhere-opensource-src-4.6.0.tar.gz).  I manually checked and sure enough its gone.


After some googling - I saw where one said that I could simply go get this package myself and put it in the /opt/freescale/pkgs directory and re-run tlib.  I did this but then I get a lot of errors with it can find the libraries (like libpng, etc...).  I verified the libraries do in fact exist.  It also gives a warning of:

"Build path taken because: directory build, no prebuilt rpm,"  and

"You have not explicitly asked to use pkg-config and are cross-compiling."

Do I need to specify in the spec file or other? where the libraries live - or is there a better way of doing this?

Thanks,

Bills

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,196件の閲覧回数
blsousan
Contributor III

Got it done by compiling QT outside of ltib.  Followed this link and had to hack at it a bit more:

http://imxcommunity.org/forum/topics/qt-4-7-4-embedded-spec-on-i-mx28

0 件の賞賛
返信

1,196件の閲覧回数
dougschwanke
Contributor IV

The link above seems to be broken.  Is there a new link to follow?

0 件の賞賛
返信