Error while flashing the board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error while flashing the board

ソリューションへジャンプ
5,052件の閲覧回数
MilanTandel
Contributor I

Flash Driver V.2 dynamic startup failed - driver Init provided no flash parameters

  Flash Driver V.2 dynamic startup failed - driver Init provided no flash parameters

  op Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPIJ driver rc 20107 (0x4E8B)

  vendor chip initialization failed - Ef(55): Dynamic flash driver startup failed to provide flash parameters.

  Debugging context: evkbmimxrt1060_lvgl_guider LinkServer Debug

0 件の賞賛
返信
1 解決策
5,024件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @MilanTandel ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   1. which board you are using?

   2. which debugger you are using?

   3. do you test the SDK project, whether that works or not?

  4. normally, this is related to your flash unmatch the flashdriver, or your flash already contains the abnormal code which prevent the boot, you need to do the flash mass erase at first, you can enter the serial download mode, use the mcubootutility to erase it, then try to download the code again.

 

Wish it helps you!

Best Regards,

Kerry

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,025件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @MilanTandel ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   1. which board you are using?

   2. which debugger you are using?

   3. do you test the SDK project, whether that works or not?

  4. normally, this is related to your flash unmatch the flashdriver, or your flash already contains the abnormal code which prevent the boot, you need to do the flash mass erase at first, you can enter the serial download mode, use the mcubootutility to erase it, then try to download the code again.

 

Wish it helps you!

Best Regards,

Kerry

0 件の賞賛
返信
5,022件の閲覧回数
MilanTandel
Contributor I
Thank you sir but it is solved and sorry i forgot to close the ticket actually There was 1 resistor which was open we short it and it worked well.
0 件の賞賛
返信