Error while executing eIQ GenAI Flow Demonstrator on advantech aom-5521(iMX95)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error while executing eIQ GenAI Flow Demonstrator on advantech aom-5521(iMX95)

2,408 Views
yuii13
Contributor II

I am getting the following ALSA error when running eiq_genai_flow with asr enabled

Currently we are using the SGTL5000 module, the system can detect it.

Is it possible to configure the default sound card?

 

root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# ./eiq_genai_flow

Target Device: i.MX95

LLM used: danube-onnx

TTS model used 16kHz quantized

ALSA lib confmisc.c:855:(parse_card) cannot find card 'default'

ALSA lib conf.c:5204:(_snd_config_evaluate) function snd_func_card_inum returned error: No such device

ALSA lib confmisc.c:422:(snd_func_concat) error evaluating strings

ALSA lib conf.c:5204:(_snd_config_evaluate) function snd_func_concat returned error: No such device

ALSA lib confmisc.c:1342:(snd_func_refer) error evaluating name

ALSA lib conf.c:5204:(_snd_config_evaluate) function snd_func_refer returned error: No such device

ALSA lib conf.c:5727:(snd_config_expand) Evaluate error: No such device

ALSA lib pcm.c:2721:(snd_pcm_open_noupdate) Unknown PCM sysdefault:CARD=default

Exception in thread Thread-5 (handle_playback):

Traceback (most recent call last):

  File "threading.py", line 1075, in _bootstrap_inner

  File "threading.py", line 1012, in run

  File "tts/model.py", line 179, in handle_playback

  File "tts/player.py", line 23, in __init__

  File "tts/player.py", line 28, in open_pcm_device

alsaaudio.ALSAAudioError: No such device [sysdefault:CARD=default]

 

 

root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# arecord -l

**** List of CAPTURE Hardware Devices ****

card 0: soundhdmi [sound-hdmi], device 0: 42670000.sai-i2s-hifi i2s-hifi-0 [42670000.sai-i2s-hifi i2s-hifi-0]

  Subdevices: 1/1

  Subdevice #0: subdevice #0

card 1: sgtl5000 [sgtl5000], device 0: HiFi sgtl5000-0 [HiFi sgtl5000-0]

  Subdevices: 1/1

  Subdevice #0: subdevice #0

root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow#

 

Tags (1)
0 Kudos
Reply
5 Replies

2,272 Views
Pierre_M
NXP Employee
NXP Employee

Hi,
As outlined in the hardware requirements, the current demo is limited to EVKs equipped with the WM8962 audio codec. That’s why it doesn’t work with other codecs like the SGTL5000.

The upcoming release, planned for this quarter,  will lift this restriction and allow the use of any codec — stay tuned!

Thanks and best regards,
Pierre

0 Kudos
Reply

2,373 Views
joanxie
NXP TechSupport
NXP TechSupport

this configure file is for audio card and device configuration, maybe you can try to set your own codec here

https://github.com/nxp-appcodehub/dm-eiq-genai-flow-demonstrator/blob/main/eiq_genai_flow/audio_conf...

0 Kudos
Reply

2,365 Views
yuii13
Contributor II

After modifying "audio_config.sh", another error message occurs

root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# ./audio_config.sh  capture
i.MX95
sysdefault:CARD=sgtl5000
Simple mixer control 'Capture',0
  Capabilities: cvolume cswitch cswitch-joined
  Capture channels: Front Left - Front Right
  Limits: Capture 0 - 15
  Front Left: Capture 15 [100%] [on]
  Front Right: Capture 15 [100%] [on]
root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# ./audio_config.sh playback
i.MX95
sysdefault:CARD=sgtl5000
Simple mixer control 'Headphone',0
  Capabilities: pvolume pswitch pswitch-joined
  Playback channels: Front Left - Front Right
  Limits: Playback 0 - 127
  Mono:
  Front Left: Playback 110 [87%] [3.50dB] [on]
  Front Right: Playback 110 [87%] [3.50dB] [on]

 

Here is the configure script I modified:

#!/bin/bash

# Copyright 2025 NXP
# NXP Proprietary.
# This software is owned or controlled by NXP and may only be used strictly in
# accordance with the applicable license terms. By expressly accepting such
# terms or by downloading, installing, activating and/or otherwise using the
# software, you are agreeing that you have read, and that you agree to comply
# with and are bound by, such license terms. If you do not agree to be bound
# by the applicable license terms, then you may not retain, install, activate
# or otherwise use the software.


audio_card_list() {
  cards=$(awk -F '[][]' '/\[.*\]/ {print $2}' /proc/asound/cards)
  echo "$cards"
}

get_audio_card() {
  supported_cards=$1
  device_cards=$2
  for s_card in $supported_cards; do
    for d_card in $device_cards; do
      if [[ "$s_card" == "$d_card" ]]; then
        echo "$d_card"
        return 1
      fi
    done
  done
  echo "default"
}

get_device() {
  # get architecture type
  arch=$(uname -m)
  soc_id=/sys/devices/soc0/soc_id
  if [ "$arch" == "x86_64" ]; then
    echo "PC"
  elif [ -f "$soc_id" ]; then
    cat $soc_id
  else
    echo "ERROR"
  fi
}

audio_setup() {
  mode=$1
  device=$(get_device)
  echo $(get_device)
  #supported_cards="wm8962audio wm8960audio"
  supported_cards="sgtl5000 wm8960audio"
  cards=$(audio_card_list)
  cur_card=$(get_audio_card "$supported_cards" "$cards")
  if [[ "$device" != "PC" ]]; then
    echo "sysdefault:CARD=$cur_card"
    if [[ $mode == "capture" ]]; then
      if [[ $cur_card == "sgtl5000" ]]; then
        amixer -c sgtl5000 sset 'Capture' 60
      elif [[ $cur_card == "wm8960audio" ]]; then
        amixer -c micfilaudio cset name='MICFIL Quality Select' 'High'
        amixer -c sgtl5000 sset 'Capture' 60
      else
        echo "'$cur_card' audio card doesn't exist"
      fi
    elif [[ $mode == "playback" ]]; then
      if [[ $cur_card == "sgtl5000" ]]; then
        amixer -c sgtl5000 set 'Headphone' 110 on
      elif [[ $cur_card == "wm8960audio" ]]; then
        amixer -c sgtl5000 set 'Headphone' 125
      else
        echo "'$cur_card' audio card doesn't exist"
      fi
    else
      echo "'$mode' mode doesn't exist use 'capture' or 'playback'"
    fi
  else # PC
    echo "$cur_card"
  fi
}

if [ $# -eq 1 ]; then
  audio_setup "$1"
else
  echo "ERROR!"
  echo "setup audio for capture or playback"
  echo "usage: audio_config.sh {capture,playback}"
fi

 

Tags (1)
0 Kudos
Reply

2,334 Views
joanxie
NXP TechSupport
NXP TechSupport

do you have any local DFAE support? currently, imx95 is still under prepordcution stage, I couldn't share any internal document or code with you, I suggest that you can contact local DFAE to get further support, and what new errors do you get? let me check if I can share anything here with you

0 Kudos
Reply

2,322 Views
yuii13
Contributor II

Here is the new error message

root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# ls
LICENSE.txt  _internal  asr  audio_config.sh  eiq_genai_flow  install.sh  llm  rag  tts
root@imx95aom5521a1:~/dm-eiq-genai-flow-demonstrator/eiq_genai_flow# ./eiq_genai_flow
Target Device: i.MX95
LLM used: danube-onnx
TTS model used 16kHz quantized
ALSA lib pcm.c:2721:(snd_pcm_open_noupdate) Unknown PCM i.MX95
Exception in thread Thread-5 (handle_playback):
Traceback (most recent call last):
  File "threading.py", line 1075, in _bootstrap_inner
  File "threading.py", line 1012, in run
  File "tts/model.py", line 179, in handle_playback
  File "tts/player.py", line 23, in __init__
  File "tts/player.py", line 28, in open_pcm_device
alsaaudio.ALSAAudioError: No such file or directory [i.MX95]

Please type your question:
0 Kudos
Reply