Error while enabling bluetooth on IMX6SL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error while enabling bluetooth on IMX6SL

3,499件の閲覧回数
mutyalaraoneela
Contributor III

Hi All,

Platform : IMX6SL

Bluedroid on Android kitkat 4.4.3.

Can you please help me I am struck at this point not able to move forward.

D/BluetoothAdapterState(  704):  CURRENT_STATE=PENDING, MESSAGE = ENABLE_TIMEOUT, isTurningOn=true, isTurningOff=false
E/BluetoothAdapterState(  704): Error enabling Bluetooth
D/BluetoothAdapterProperties(  704): Setting state to 10
I/BluetoothAdapterState(  704): Bluetooth adapter state changed: 11-> 10
D/BluetoothAdapterService(  704): Broadcasting updateAdapterState() to 1 receivers.

what's wrong with this..... Not getting any idea. Please help me.....

Thanks and regards,

MutyalaRao.

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,204件の閲覧回数
mutyalaraoneela
Contributor III

Hi Hasssan khan,

  This issue basically comes when the communication is not proper in between your bluetooth driver and Bluedroid stack.

May I know your driver details??

0 件の賞賛
返信

3,204件の閲覧回数
hassankhan
Contributor I

Hi mutyalaraoneelapala,

Thanks for your reply ...

we are using Dialog DA14580 and trying to implement it in android (kitrkat) using bluedroid

we tried to implement it using uart interface and able to download firmware to device(since acording to vendor they dont have separate driver, firmware should take care of that) but after that we got stuck and unable to proceed

For detail you can ref below link:

http://support.dialog-semiconductor.com/how-download-firmware-da14580-ble-chip

regards,

Hassan khan

0 件の賞賛
返信

3,204件の閲覧回数
hassankhan
Contributor I

Hi mutyalaraoneelapala​,

I am facing simlar issue ,

Platform : IMX6SL

Bluedroid on Android kitkat 4.4.3.

Can you please help me I am struck at this point not able to move forward.

D/BluetoothAdapterState(  704):  CURRENT_STATE=PENDING, MESSAGE = ENABLE_TIMEOUT, isTurningOn=true, isTurningOff=false
E/BluetoothAdapterState(  704): Error enabling Bluetooth
D/BluetoothAdapterProperties(  704): Setting state to 10
I/BluetoothAdapterState(  704): Bluetooth adapter state changed: 11-> 10
D/BluetoothAdapterService(  704): Broadcasting updateAdapterState() to 1 receivers.

Thanks and regards,

Hasssan khan

0 件の賞賛
返信

3,205件の閲覧回数
mutyalaraoneela
Contributor III

Hi all,

  After enabling bluetooth, while transferring file from third party mobile to IMX_6SL board, file is getting transferred(TX), but vice versa (RX) is not happening, it is giving the error message :

   File not Received

   File : sample.jpg

   Reason : Storage issue

  Please suggest me how to proceed further???

0 件の賞賛
返信

3,205件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Mutyalarao,

What type of bluetooth adapter are you using?

0 件の賞賛
返信