Error while downloading through MFGtool in IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error while downloading through MFGtool in IMX6

1,284 Views
asmaalekar90
Contributor I

Hello Everyone,

I am trying to download uboot on our custom board which uses mcimx6g3cvm05ab IC through MFGtool. I am using mfgtool2-yocto-mx-evk-emmc.vbs script from L4.1.15_2.0.0-ga_mfg-tools to download on our board. MFGtool stuck while downloading U-boot and it is giving me following error. Can someone please point me if I am doing anything wrong?

ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is C:\Users\asmaa\Desktop\L4.1.15_2.0.0-ga_mfg-tools.tar\L4.1.15_2.0.0-ga_mfg-tools\mfgtools-with-rootfs.tar\mfgtools-with-rootfs\mfgtools\Profiles\linux\OS Firmware\firmware\u-boot-imx6ul14x14evk_emmc.imx
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: ExecuteCommand--Load[WndIndex:0], File is C:\Users\asmaa\Desktop\L4.1.15_2.0.0-ga_mfg-tools.tar\L4.1.15_2.0.0-ga_mfg-tools\mfgtools-with-rootfs.tar\mfgtools-with-rootfs\mfgtools\Profiles\linux\OS Firmware\firmware\zImage, address is 0x80800000
ModuleID[2] LevelID[10]: PortMgrDlg(0)--Command Load excute successfully, retry count: 0
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: ExecuteCommand--Load[WndIndex:0], File is C:\Users\asmaa\Desktop\L4.1.15_2.0.0-ga_mfg-tools.tar\L4.1.15_2.0.0-ga_mfg-tools\mfgtools-with-rootfs.tar\mfgtools-with-rootfs\mfgtools\Profiles\linux\OS Firmware\firmware\fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot, address is 0x83800000
ModuleID[2] LevelID[10]: PortMgrDlg(0)--Command Load excute successfully, retry count: 0
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: ExecuteCommand--Load[WndIndex:0], File is C:\Users\asmaa\Desktop\L4.1.15_2.0.0-ga_mfg-tools.tar\L4.1.15_2.0.0-ga_mfg-tools\mfgtools-with-rootfs.tar\mfgtools-with-rootfs\mfgtools\Profiles\linux\OS Firmware\firmware\zImage-imx6ul-14x14-evk-emmc.dtb, address is 0x83000000
ModuleID[2] LevelID[10]: PortMgrDlg(0)--Command Load excute successfully, retry count: 0
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: ExecuteCommand--Jump[WndIndex:0]
ModuleID[2] LevelID[10]: *********MxHidDevice[02F11160] Jump to Ramkernel successfully!**********
ModuleID[2] LevelID[10]: CmdOperation[0], current state command has been finished and the last command is successful, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 0
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)
ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is C:\Users\asmaa\Desktop\L4.1.15_2.0.0-ga_mfg-tools.tar\L4.1.15_2.0.0-ga_mfg-tools\mfgtools-with-rootfs.tar\mfgtools-with-rootfs\mfgtools\Profiles\linux\OS Firmware\firmware\u-boot-imx6ul14x14evk_emmc.imx
ModuleID[2] LevelID[1]: MxHidDevice::Read() Error reading from device 0x48f.
ModuleID[2] LevelID[10]: DeviceManager::DevChangeWnd::OnDeviceChange() - DEVICE_REMOVAL_EVT(\\?\USB#VID_15A2&PID_007D#5&182cd075&0&1#{a5dcbf10-6530-11d2-901f-00c04fb951ed})
ModuleID[2] LevelID[1]: Failed to read HAB type from ROM!!!
ModuleID[2] LevelID[1]: Failed to initialize memory!
ModuleID[2] LevelID[10]: DeviceManager::DevChangeWnd::OnDeviceChange() - end
ModuleID[2] LevelID[1]: PortMgrDlg(0)--MxHidDevice--Command Boot excute failed
ModuleID[2] LevelID[10]: DeviceManager::OnMsgDeviceEvent() - DEVICE_REMOVAL_EVT(\\?\USB#VID_15A2&PID_007D#5&182cd075&0&1#{a5dcbf10-6530-11d2-901f-00c04fb951ed})
ModuleID[2] LevelID[10]: DeviceClass::FindDeviceByUsbPath--DeviceListType_Current, _devices.size: 1
ModuleID[2] LevelID[10]: DeviceClass::FindDeviceByUsbPath--DeviceListType_Current, devInstPathToFind: USB\VID_15A2&PID_007D\5&182CD075&0&1, _deviceInstanceID: USB\VID_15A2&PID_007D\5&182CD075&0&1
ModuleID[2] LevelID[10]: DeviceClass::FindDeviceByUsbPath--DeviceListType_Current, Find the device

Regards,

Sabrina

Labels (1)
0 Kudos
Reply
1 Reply

1,150 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Asma,

Did you apply the proper changes to use MFGTool on a custom board? Please refer to the following Community thread for additional details:

How to use use MFG tool for the custom board. 


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply