Error while building for  imx-image-full

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error while building for  imx-image-full

1,276件の閲覧回数
ShivM
Contributor II

Hi ,

I am trying build for imx-image-full and getting below error

 

WARNING: imx-gpu-viv-1_6.4.3.p1.2-aarch64-r0 do_fetch: Failed to fetch URL https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.3.p1.2-aarch64.bin;fsl-eula=true, attempting MIRRORS if available
ERROR: imx-gpu-viv-1_6.4.3.p1.2-aarch64-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/731871/bus"; export http_proxy="http://approxy.removednamed:9090/"; export PATH="/linuxbuilds/imx-yocto-bsp/sources/poky/scripts:/linuxbuilds/imx-yocto-bsp/build/tmp/work/cortexa53-crypto-mx8mp-poky-linux/imx-gpu-viv/1_6.4.3.p1.2-aarch64-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/linuxbuilds/imx-yocto-bsp/build/tmp/work/cortexa53-crypto-mx8mp-poky-linux/imx-gpu-viv/1_6.4.3.p1.2-aarch64-r0/recipe-sysroot/usr/bin/crossscripts:/linuxbuilds/imx-yocto-bsp/build/tmp/work/cortexa53-crypto-mx8mp-poky-linux/imx-gpu-viv/1_6.4.3.p1.2-aarch64-r0/recipe-sysroot-native/usr/sbin:/linuxbuilds/imx-yocto-bsp/build/tmp/work/cortexa53-crypto-mx8mp-poky-linux/imx-gpu-viv/1_6.4.3.p1.2-aarch64-r0/recipe-sysroot-native/usr/bin:/linuxbuilds/imx-yocto-bsp/build/tmp/work/cortexa53-crypto-mx8mp-poky-linux/imx-gpu-viv/1_6.4.3.p1.2-aarch64-r0/recipe-sysroot-native/sbin:/linuxbuilds/imx-yocto-bsp/build/tmp/work/cortexa53-crypto-mx8mp-poky-linux/imx-gpu-viv/1_6.4.3.p1.2-aarch64-r0/recipe-sysroot-native/bin:/linuxbuilds/imx-yocto-bsp/sources/poky/bitbake/bin:/linuxbuilds/imx-yocto-bsp/build/tmp/hosttools"; export HOME="/accts/smaddani"; /usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate -P /linuxbuilds/imx-yocto-bsp/downloads/ 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.3.p1.2-aarch64.bin' --progress=dot -v failed with exit code 4, output:
--2021-07-21 12:56:19-- https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.3.p1.2-aarch64.bin
Resolving www.nxp.com (www.nxp.com)... 96.6.65.45
Connecting to www.nxp.com (www.nxp.com)|96.6.65.45|:443... failed: Connection timed out.
Retrying.

--2021-07-21 12:56:50-- (try: 2) https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.3.p1.2-aarch64.bin
Connecting to www.nxp.com (www.nxp.com)|96.6.65.45|:443... failed: Connection timed out.
Giving up.


ERROR: imx-gpu-viv-1_6.4.3.p1.2-aarch64-r0 do_fetch: Fetcher failure for URL: 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.3.p1.2-aarch64.bin;fsl-eula=true'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /linuxbuilds/imx-yocto-bsp/build/tmp/work/cortexa53-crypto-mx8mp-poky-linux/imx-gpu-viv/1_6.4.3.p1.2-aarch64-r0/temp/log.do_fetch.995331
ERROR: Task (/linuxbuilds/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-graphics/imx-gpu-viv/imx-gpu-viv_6.4.3.p1.2-aarch64.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1052 tasks of which 1046 didn't need to be rerun and 1 failed.

Summary: 1 task failed:

0 件の賞賛
返信
1 返信

1,269件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello ShivM,

 

Erase everything and try again to download the imx-image-full, i Just tested and it works.

Regards

0 件の賞賛
返信