Error reading cluster for SD card boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error reading cluster for SD card boot

3,388 次查看
t2865k5
Contributor I

Dear NXP ,

 

U-Boot version : 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)

HW platform: srg-imx8mplus (base on imx8mplus)

Memory : MT53D512M32D2 (2GB)

SD card : SP 16GB and SanDisk 16GB

 

Build a bootable SD card for imx8mplus platform . Use the SD card to boot in srg-imx8mplus platform .

In Uboot mode , this message is as follows:

switch to partitions #0, OK
mmc1 is current device
Error reading cluster

 

It can't boot normally form SD card. Please help to fix this issue.

 

t2865k5_0-1657000929742.png

 

标签 (1)
0 项奖励
回复
2 回复数

3,370 次查看
t2865k5
Contributor I

Dear NXP ,

This issue needs to be resolved as soon as possible. I have been waiting for a very long time ,and I hope you can help us resolve this issue.

0 项奖励
回复

3,000 次查看
www1519
Contributor III

Dear  t2865k5

Has the problem been solved? What countermeasures is it.

The same trouble has happened. 

0 项奖励
回复