Error in Creating baremetal project for asrc- fatal error: asrc_common.h: No such file or directory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error in Creating baremetal project for asrc- fatal error: asrc_common.h: No such file or directory

1,985 次查看
akk1
Contributor I

Hi,

I want to create baremetal project for using hardware asrc in imx6ul board. I am using processor expert tool. I got some reference code for asrc barmetal from the imx6ul reference manual in chapter 16. The code needs header files asrc_common.h, soc_api.h and wy_ideal_ratio_dataini_part.h. When I compile the code, I am getting the errors that there are no such files. Can someone please help me where I can get these header files. Do they come with Processor expert tool package? Thanks in advance..

Thanks

ankit

标签 (2)
标记 (3)
0 项奖励
回复
1 回复

1,313 次查看
igorpadykov
NXP Employee
NXP Employee

HI ankit

these headers are for simulation software and I am afraid not

available. For asrc example one can look at linux driver, described

in Chapter 30 Asynchronous Sample Rate Converter (ASRC)

Driver attached Linux Manual.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复