i.MX6 MLC nand support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 MLC nand support

1,527 Views
ranjithhebbar
Contributor II
Dear All,
     How emmc MLC nand support power loss protection in i.MX6 platform..?
          Does Micron e.MMC support power-loss protection?

Yes, ESG e.MMC devices support static data protection. Devices are shipped from Micron factories as COMBO with a configuration optimized for best write performance. Customers can reconfigure the devices to protect static (previously written) data if there is power loss during a write operation.

How to reconfigure the device during power loss.

0 Kudos
Reply
3 Replies

1,273 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

procedure is described in Micron app note

TN-FC-27: e.MMC Power Loss Data Integrity

https://www.micron.com/support/document-search?document_type={A4B84EF3-C609-451A-9264-74A4A2B6F5E4}&view=all

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,273 Views
ranjithhebbar
Contributor II

Hi igor,

    Thanks for your useful information.

     How we can take care Partition protection and reliable write in our i.MX6 linux BSP. support is there...?

Best Regards,

Ranjith hebbar

0 Kudos
Reply

1,273 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

I think not, but you can add such support using that app note.

~igor

0 Kudos
Reply