Error during debug of Motor control software in MIMXRT1060

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error during debug of Motor control software in MIMXRT1060

886 次查看
AnweshaPanda
NXP Employee
NXP Employee

I downloaded the latest motor control software example from SDK store. I can build it but it encounters error bus fault ( while debug. See picture. Please suggest a solution. 

AnweshaPanda_0-1631002409171.png

 

AnweshaPanda_0-1631003262086.png

 

 

0 项奖励
回复
1 回复

872 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello AnweshaPanda,

The mc_pmsm example requires some hardware setup, which can be found on the Application User’s Guide which is mentioned on the example readme under the doc folder.

The user guide does include the hardware setup for the i.MXRT1060-EVK, which includes some jumper settings and placing some resistors on the bottom side of the board. I would start by double checking that all the hardware is setup correctly.

Regards,
Gustavo

0 项奖励
回复