Error during bitbake fsl-image-gui for imx6ulevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error during bitbake fsl-image-gui for imx6ulevk

6,302 Views
freescale_jive
Contributor II

Hi,

I followed the "Freescale_Yocto_Project_User's_Guide.pdf" to setup the PC host and yocto, and eventually trying to run:

$> bitbake fsl-image-gui

But I received the following error. What have I missed? Thanks!

===========================

ERROR:

ERROR: ld.so: object 'libpseudo.so' from LD_PRELOAD cannot be preloaded (wrong ELF class: ELFCLASS64): ignored.

Adding system startup for /home/adsuser/work/02_fsl-release-bsp/build-fb03/tmp/work/imx6ulevk-poky-linux-gnueabi/fsl-image-gui/1.0-r0/rootfs/etc/init.d/avahi-daemon.

Output from lttng-tools-2.6.0-r0@cortexa7hf_vfp_neon:

Running groupadd commands...

NOTE: Performing groupadd with [--root /home/adsuser/work/02_fsl-release-bsp/build-fb03/tmp/work/imx6ulevk-poky-linux-gnueabi/fsl-image-gui/1.0-r0/rootfs tracing] and 10 times of retry

ERROR: Function failed: do_rootfs

ERROR: Logfile of failure stored in: /home/adsuser/work/02_fsl-release-bsp/build-fb03/tmp/work/imx6ulevk-poky-linux-gnueabi/fsl-image-gui/1.0-r0/temp/log.do_rootfs.8597

ERROR: Task 7 (/home/adsuser/work/02_fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-gui.bb, do_rootfs) failed with exit code '1'

NOTE: Tasks Summary: Attempted 4180 tasks of which 4137 didn't need to be rerun and 1 failed.

No currently running tasks (4180 of 4181)

Summary: 1 task failed:

  /home/adsuser/work/02_fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-gui.bb, do_rootfs

Summary: There were 5 WARNING messages shown.

Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

========================================================================

- Thomas

Labels (3)
Tags (2)
9 Replies

4,141 Views
m_eicher
Contributor II

Hello Gusarambula

I have a similar problem with building images for imx6ulevk.

The images 'core-image-minimal' and 'core-image-base' were built successfully. But the image build 'fsl-image-machine-test' failed with error:

ERROR: Task 3968 (virtual:native:/home/michael/fsl-arm-yocto-bsp/sources/poky/meta/recipes-devtools/qemu/qemu_2.2.0.bb, do_configure) failed with exit code '1'

Above there was another error message:

| ERROR: User requested feature sdl

|                 configure was not able to find it.

|                 Install SDL devel

The yocto runs on Ubuntu 15.10. I did the installation exactly from 'Freescale Yocto Project User's Guide'.

Regards

Michael

0 Kudos
Reply

4,141 Views
1990rahulreddy
Contributor IV

from this , Yocto Project Reference Manual

follow 1.3.2 and

1.3.3.1.

for ubuntu 14.04

4,141 Views
m_eicher
Contributor II

Hi Rahul

Thank you for your answer.

I reinstalled libsdl1.2-dev and I followed the instructions 1.3.2 and 1.3.3.1

Nothing helped. Still the same error.

Regards

Michael

4,141 Views
1990rahulreddy
Contributor IV

Remove everything..i mean directory created..by download..

& install everything with HIGH SPEED INTERNET Connection...

4,141 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Michael Eicher,

Have you installed all required packages correctly? The error may be related with the libsdl1.2-dev package, that is required by the host.

Regards,

0 Kudos
Reply

4,141 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Thomas,

I’m trying to duplicate the issue . In the meantime, would you please share the steps you performed and the local.conf file? Does it have the correct MACHINE variable and the EULA set to 1?

0 Kudos
Reply

4,141 Views
freescale_jive
Contributor II

Hello Gusarambula,

I've followed exactly the steps described in "Freescale_Yocto_Project_User's_Guide.pdf".

After successfully "repo sync", I executed the following commands:

$> MACHINE=imx6ulevk source fsl-setup-release.sh -b build-fb03 -e fb

$> bitbake fsl-image-gui

The content of conf/local.conf is:

MACHINE ??= 'imx6ulevk'

DISTRO ?= 'fsl-imx-release-fb'

PACKAGE_CLASSES ?= "package_rpm"

EXTRA_IMAGE_FEATURES = "debug-tweaks"

USER_CLASSES ?= "buildstats image-mklibs image-prelink"

PATCHRESOLVE = "noop"

BB_DISKMON_DIRS = "\

    STOPTASKS,${TMPDIR},1G,100K \

    STOPTASKS,${DL_DIR},1G,100K \

    STOPTASKS,${SSTATE_DIR},1G,100K \

    ABORT,${TMPDIR},100M,1K \

    ABORT,${DL_DIR},100M,1K \

    ABORT,${SSTATE_DIR},100M,1K"

PACKAGECONFIG_append_pn-qemu-native = " sdl"

PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"

ASSUME_PROVIDED += "libsdl-native"

CONF_VERSION = "1"

BB_NUMBER_THREADS = '4'

PARALLEL_MAKE = '-j 4'

DL_DIR ?= "${BSPDIR}/downloads/"

ACCEPT_FSL_EULA = "1"

- Thomas

0 Kudos
Reply

4,141 Views
freescale_jive
Contributor II

By the way, the PC host I used is Ubuntu 14.04LTS.

- Thomas

0 Kudos
Reply

4,141 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Thomas,

It's odd because I was able to build with no problems so the sources should be in place.

I'm using Ubuntu 12.04 but 14.04 should also work. Would you please double check that you have the necessary packages. Please also try either from a new build directory or after making a clean:

bitbake -c cleanall fsl-image-gui

0 Kudos
Reply