Error comes while debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error comes while debugging

1,344 Views
sajithdevidas
Contributor III

I'm, using rt1170 board with mcuexpresso, and im getting these erroes while i'm debbugging, please help and tell how to ovecome this?

 

 

MCUXpresso IDE RedlinkMulti Driver v11.8 (Jul 12 2023 16:09:15 - crt_emu_cm_redlink build 2)

Found chip XML file in C:/nxp/SLEEP_WAKEUP_WORKSPACE/SLEEP_WAKEUP_EVK/Debug\MIMXRT1176xxxxx.xml

( 5) Remote configuration complete

Reconnected to existing LinkServer process.

============= SCRIPT: RT1170_connect_M7_wake_M4.scp =============

RT1170 Connect M7 and Wake M4 Script

DpID = 6BA02477

Error: Wire Ack Fault - target connected?

Setting M4 spin code

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Setting M4 clock

Error: Wire Ack Fault - target connected?

Resetting M4 core

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

View cores on the DAP AP

DpID = 6BA02477

TAP 0: 6BA02477 Core 1: M4 APID: 24770011 ROM Table: E00FF003

Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

============= END SCRIPT ========================================

Probe Firmware: MCU-LINK r0FF CMSIS-DAP V0.078 (NXP Semiconductors)

Serial Number: E4AO4L4PRLOU1

VID:PID: 1FC9:0143

USB Path: \\?\hid#vid_1fc9&pid_0143&mi_00#7&1d2ef268&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}

Using memory from core 0 after searching for a good core

Using memory from core 0 after searching for a good core

Using memory from core 0 after searching for a good core

connection failed - Nn(05). Wire ACK Fault in DAP access.. Retrying

Using memory from core 0 after searching for a good core

Using memory from core 0 after searching for a good core

Using memory from core 0 after searching for a good core

Failed on connect: Nn(05). Wire ACK Fault in DAP access

Connected&Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000000. Info: <None>

Last stub error 0: OK

Last sticky error: 0x0 AIndex: 0

Debug bus selected: MemAp 0

DAP Speed test unexecuted or failed

Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.

(100) Target Connection Failed

error closing down debug session - Nn(05). Wire ACK Fault in DAP access

 

 

0 Kudos
Reply
1 Reply

1,277 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sajithdevidas 

Do you use DEMO board? If yes, please refer to start guide to download and debug:

https://www.nxp.com/document/guide/getting-started-with-the-i-mx-rt1170-evaluation-kit:GS-MIMXRT1170... 

Also pay attention jumpers on board, recommend use a simple SDK demo first to test.

 

BR

Alice

0 Kudos
Reply