Error building yocto project image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error building yocto project image

Jump to solution
2,801 Views
waynetsui
Contributor II

BSP: imx-3.14.28-1.0.0_ga

0 Kudos
Reply
1 Solution
1,626 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wayne Tsui,

It is most likely that the problem resides in that you’re using the FSL BSP Release and not the FSL Community BSP. The former does not support the RioTboard and that’s why the image cannot be built for that target.

Please download the FSL Community BSP and try baking the image for the RioTboard with it. There is information on where to download it on the following link:

FSL Community BSP

View solution in original post

0 Kudos
Reply
3 Replies
1,626 Views
waynetsui
Contributor II

$ MACHINE=imx6dl-riotboard  source fsl-setup-release.sh -b RIoTboard -e fb

$ bitbake  -k core-image-minimal

ERROR: Function failed: do_compile (log file is located at /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021)

ERROR: Logfile of failure stored in: /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021

Log data follows:

| DEBUG: Executing shell function do_compile

| NOTE: make -j 3 CROSS_COMPILE=arm-poky-linux-gnueabi- CC=arm-poky-linux-gnueabi-gcc  --sysroot=/home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/sysroots/imx6dl-riotboard riotboard_defconfig

| make: *** No rule to make target `riotboard_defconfig'.  Stop.

| ERROR: oe_runmake failed

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_compile (log file is located at /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021)

ERROR: Task 238 (/home/wayne/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2014.04.bb, do_compile) failed with exit code '1'

WARNING: QA Issue: pulseaudio-module-console-kit rdepends on consolekit, but it isn't a build dependency? [build-deps]

Currently 1 running tasks (2008 of 2036):

0: linux-imx-3.14.28-r0 do_fetch (pid 15820)

0 Kudos
Reply
1,627 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wayne Tsui,

It is most likely that the problem resides in that you’re using the FSL BSP Release and not the FSL Community BSP. The former does not support the RioTboard and that’s why the image cannot be built for that target.

Please download the FSL Community BSP and try baking the image for the RioTboard with it. There is information on where to download it on the following link:

FSL Community BSP

0 Kudos
Reply
1,626 Views
waynetsui
Contributor II

Thank you , gusarambula.

0 Kudos
Reply