Error building yocto project image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error building yocto project image

跳至解决方案
2,945 次查看
waynetsui
Contributor II

BSP: imx-3.14.28-1.0.0_ga

0 项奖励
回复
1 解答
1,770 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wayne Tsui,

It is most likely that the problem resides in that you’re using the FSL BSP Release and not the FSL Community BSP. The former does not support the RioTboard and that’s why the image cannot be built for that target.

Please download the FSL Community BSP and try baking the image for the RioTboard with it. There is information on where to download it on the following link:

FSL Community BSP

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,770 次查看
waynetsui
Contributor II

$ MACHINE=imx6dl-riotboard  source fsl-setup-release.sh -b RIoTboard -e fb

$ bitbake  -k core-image-minimal

ERROR: Function failed: do_compile (log file is located at /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021)

ERROR: Logfile of failure stored in: /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021

Log data follows:

| DEBUG: Executing shell function do_compile

| NOTE: make -j 3 CROSS_COMPILE=arm-poky-linux-gnueabi- CC=arm-poky-linux-gnueabi-gcc  --sysroot=/home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/sysroots/imx6dl-riotboard riotboard_defconfig

| make: *** No rule to make target `riotboard_defconfig'.  Stop.

| ERROR: oe_runmake failed

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_compile (log file is located at /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021)

ERROR: Task 238 (/home/wayne/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2014.04.bb, do_compile) failed with exit code '1'

WARNING: QA Issue: pulseaudio-module-console-kit rdepends on consolekit, but it isn't a build dependency? [build-deps]

Currently 1 running tasks (2008 of 2036):

0: linux-imx-3.14.28-r0 do_fetch (pid 15820)

0 项奖励
回复
1,771 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wayne Tsui,

It is most likely that the problem resides in that you’re using the FSL BSP Release and not the FSL Community BSP. The former does not support the RioTboard and that’s why the image cannot be built for that target.

Please download the FSL Community BSP and try baking the image for the RioTboard with it. There is information on where to download it on the following link:

FSL Community BSP

0 项奖励
回复
1,770 次查看
waynetsui
Contributor II

Thank you , gusarambula.

0 项奖励
回复