Error building the XIP image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error building the XIP image

1,022件の閲覧回数
nishad_kamdar
Contributor IV

Hi,

I have a very resource constraint application which uses a custom iMX6 board.

I am using the parallel NOR flash for booting the kernel.

I tried using the XIP image for executing the Kernel directly form the NOR.

However it has the !ZBOOT_ROM constraint which i am not able to find anywhere in the boot option sin LTIB.

i am using the L3.0.35_4.1.0 kernel version by the way.

According the the help i need to manually provide the BSS and the text addresses of the image to be loaded in the kernel.

Can anyone tell me what is the default place in the NOR where the BSS and the text sections of the UImage are loaded?

regards,

nishad

0 件の賞賛
返信
1 返信

919件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Hardly our Linux kernel can be built to work directly from NOR without DRAM memory.
We do not have such experience.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信