Error building in mkimage_imx8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error building in mkimage_imx8

4,355件の閲覧回数
edwardbong
Contributor II

Hi

I was building for my custom board project and believed I had done most of the duplicates of the 

EVK codes and edited the relevant Kconfig and makefiles.

One thing I has problem solving is the below build error which I think is most likely

from the IMXBOOT_TARGETS="flash_pci flash_pci_no_hdmi" from my machine file. 

Any replies is welcome.

The error message are as follows :

Log data follows:
| DEBUG: Executing shell function do_compile
| 8MQ boot binary build
| Copy ddr_firmware: lpddr4_pmu_train_1d_imem.bin from /home/et/imx8-pci-004/build-001/tmp/deploy/images/imx8mq-pci -> /home/et/imx8-pci-004/build-001/tmp/work/imx8mq_pci-poky-linux/imx-boot/0.2-r0/git/iMX8M
| Copy ddr_firmware: lpddr4_pmu_train_1d_dmem.bin from /home/et/imx8-pci-004/build-001/tmp/deploy/images/imx8mq-pci -> /home/et/imx8-pci-004/build-001/tmp/work/imx8mq_pci-poky-linux/imx-boot/0.2-r0/git/iMX8M
| Copy ddr_firmware: lpddr4_pmu_train_2d_imem.bin from /home/et/imx8-pci-004/build-001/tmp/deploy/images/imx8mq-pci -> /home/et/imx8-pci-004/build-001/tmp/work/imx8mq_pci-poky-linux/imx-boot/0.2-r0/git/iMX8M
| Copy ddr_firmware: lpddr4_pmu_train_2d_dmem.bin from /home/et/imx8-pci-004/build-001/tmp/deploy/images/imx8mq-pci -> /home/et/imx8-pci-004/build-001/tmp/work/imx8mq_pci-poky-linux/imx-boot/0.2-r0/git/iMX8M
| building iMX8M - flash_pci
| Compiling mkimage_imx8
| make[1]: *** No rule to make target `flash_pci'. Stop.
| make: *** [flash_pci] Error 2
| WARNING: exit code 2 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/et/imx8-pci-004/build-001/tmp/work/imx8mq_pci-poky-linux/imx-boot/0.2-r0/temp/log.do_compile.9862)
ERROR: Task (/home/et/imx8-pci-004/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/imx-mkimage/imx-boot_0.2.bb:do_compile) failed with exit code '1'

regards, Edward

ラベル(2)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

3,695件の閲覧回数
2046880190
Contributor III

你好

   我也遇上了这个问题,请问你解决了么?

   我遇上过两次,因为我对yocto所有内容有备份,所以我可以直接替换一下。

   但是替换时间太长,想找到更快的解决方法。

0 件の賞賛
返信

3,695件の閲覧回数
edwardbong
Contributor II

应该是放弃了。帮不了你。抱歉。

On Tue, 25 Jun 2019, 11:03 [email protected], <[email protected]>

0 件の賞賛
返信

3,695件の閲覧回数
2046880190
Contributor III

谢谢!!

0 件の賞賛
返信