Error: The image creation script

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error: The image creation script

2,962 Views
niranjanbc
Contributor IV

i have build working fine on two Linux PC's and failing one PC. same source and yocto build.

what could be the issue.

NOTE: Running image creation script for tar: /home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.tar ...
NOTE: Creating symlinks for squashfs image ...
NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.squashfs -> core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.squashfs
NOTE: Creating symlinks for ext3 image ...
NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.ext3 -> core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.ext3
NOTE: Creating symlinks for tar image ...
NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.tar.bz2 -> core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.tar.bz2
NOTE: Running image creation script for sdcard: /home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.sdcard ...
ERROR: Error: The image creation script '/home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.sdcard' returned 1:
0+0 records in
0+0 records out
0 bytes (0 B) copied, 2.083e-05 s, 0.0 kB/s
Model: (file)
Disk /home/niranjan/fsl-community-bsp/build_emmc/tmp/deploy/images/phx-core-pca/core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.sdcard: 302MB
Sector size (logical/physical): 512B/512B
Partition Table: msdos
Disk Flags:

Number Start End Size Type File system Flags
1 4194kB 12.6MB 8389kB primary lba
2 12.6MB 298MB 285MB primary

758+0 records in
758+0 records out
388096 bytes (388 kB) copied, 0.000897308 s, 433 MB/s
mkfs.vfat 2.11 (12 Mar 2005)
WARNING: exit code 1 from a shell command.

DEBUG: Python function do_rootfs finished
ERROR: Function failed: do_rootfs

Labels (6)
Tags (2)
0 Kudos
Reply
2 Replies

2,770 Views
niranjanbc
Contributor IV

i am using Ubuntu 14.04, it is same across all the machines

i am using fido branch bsp.

0 Kudos
Reply

2,770 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello niranjanbc,

Would you please provide more details on what hosts are you using? The Yocto NXP works with Ubuntu as that is the preferred host OS. Using other OS may cause errors as some packages are not available to older or newer BSPs.

Would you please also comment what specific BSP are you using?

Regards,

0 Kudos
Reply