Error: The image creation script

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error: The image creation script

2,948件の閲覧回数
niranjanbc
Contributor IV

i have build working fine on two Linux PC's and failing one PC. same source and yocto build.

what could be the issue.

NOTE: Running image creation script for tar: /home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.tar ...
NOTE: Creating symlinks for squashfs image ...
NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.squashfs -> core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.squashfs
NOTE: Creating symlinks for ext3 image ...
NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.ext3 -> core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.ext3
NOTE: Creating symlinks for tar image ...
NOTE: Creating symlink: core-image-phx-core-pca-phx-core-pca.tar.bz2 -> core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.tar.bz2
NOTE: Running image creation script for sdcard: /home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.sdcard ...
ERROR: Error: The image creation script '/home/niranjan/fsl-community-bsp/build_emmc/tmp/work/phx_core_pca-poky-linux-gnueabi/core-image-phx-core-pca/1.0-r0/temp/create_image.sdcard' returned 1:
0+0 records in
0+0 records out
0 bytes (0 B) copied, 2.083e-05 s, 0.0 kB/s
Model: (file)
Disk /home/niranjan/fsl-community-bsp/build_emmc/tmp/deploy/images/phx-core-pca/core-image-phx-core-pca-phx-core-pca-20180108114647.rootfs.sdcard: 302MB
Sector size (logical/physical): 512B/512B
Partition Table: msdos
Disk Flags:

Number Start End Size Type File system Flags
1 4194kB 12.6MB 8389kB primary lba
2 12.6MB 298MB 285MB primary

758+0 records in
758+0 records out
388096 bytes (388 kB) copied, 0.000897308 s, 433 MB/s
mkfs.vfat 2.11 (12 Mar 2005)
WARNING: exit code 1 from a shell command.

DEBUG: Python function do_rootfs finished
ERROR: Function failed: do_rootfs

ラベル(6)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,756件の閲覧回数
niranjanbc
Contributor IV

i am using Ubuntu 14.04, it is same across all the machines

i am using fido branch bsp.

0 件の賞賛
返信

2,756件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello niranjanbc,

Would you please provide more details on what hosts are you using? The Yocto NXP works with Ubuntu as that is the preferred host OS. Using other OS may cause errors as some packages are not available to older or newer BSPs.

Would you please also comment what specific BSP are you using?

Regards,

0 件の賞賛
返信