Error: DAP error while reading AIRCR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error: DAP error while reading AIRCR

ソリューションへジャンプ
5,689件の閲覧回数
SakSath
Contributor III

Hi,

 

I am trying to connect to i.mx 1170EVK from Jlink and started facing this issue 

Error: DAP error while reading AIRCR

The issue has randomly popped up and I tried solutions like "unlocking kinetis" - but nothing worked.

I was able to connect to the board properly multiple times before this error popped up.

Also I have tried re booting the board using LPC scrypt.

Any solution / workaround is highly appreciated.

Thanks!

0 件の賞賛
返信
1 解決策
5,680件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @SakSath ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, I hope you can share the screenshot of the error, next, you can try the below trick to recover.
) Set the SW1 to Serial Downloader.
2) Power on the board, and debug the demo project.
3) After that, power off and recover the SW1 to the previous set, then power on again.
4) Give a debug again.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,681件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @SakSath ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, I hope you can share the screenshot of the error, next, you can try the below trick to recover.
) Set the SW1 to Serial Downloader.
2) Power on the board, and debug the demo project.
3) After that, power off and recover the SW1 to the previous set, then power on again.
4) Give a debug again.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
5,678件の閲覧回数
SakSath
Contributor III

Hi @jeremyzhou ,

Thanks a lot for the prompt support! The above solution worked!

 

 

0 件の賞賛
返信