Hi Yuri:
The problem we encountered was that the system received serial port input during boot, which interrupted the normal startup process of the Uboot .
The uboot we used is U-Boot 2020.04 and the Linux version is 5.4.70
U-Boot 2020.04-gbc8a51b (Feb 21 2022 - 17:11:20 +0800)
CPU: i.MX8MNano Quad rev1.0 at 1200 MHz
Reset cause: POR
Model: NXP i.MX8MNano LPDDR4 EVK board
DRAM: 1 GiB
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
BuildInfo:
- ATF f1d7187
- U-Boot 2020.04-gbc8a51b
switch to partitions #0, OK
mmc2(part 0) is current device
Net: No ethernet found.
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
u-boot=> gfhg
Unknown command 'gfhg' - try 'help'
u-boot=>