Encrypted storage using CAAM on linux-imx v5.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Encrypted storage using CAAM on linux-imx v5.4

2,635件の閲覧回数
fahad_arslan
Contributor II

Following app note is based on linux-imx v4.14 and has patches applicable to kernel v4.14.

https://www.nxp.com/docs/en/application-note/AN12714.pdf 

How can storage encryption using CAAM be done using linux-imx v5.4?

Thanks,

Fahad

3 返答(返信)

2,542件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You directly some comments.

Regards,

Yuri.

0 件の賞賛
返信

2,434件の閲覧回数
kile964
Contributor II

Hello Yuri,

Can you share this information with me as well?

0 件の賞賛
返信

2,536件の閲覧回数
aleksandar_niko
Contributor III

Hello Yuri,

could you share the same info with me as I am also working on the same thing (rootfs encryption with 5.4 Linux from initramfs).

Best,

Aleksandar

0 件の賞賛
返信