Encrypted Storage Using CAAM Secure Keys

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Encrypted Storage Using CAAM Secure Keys

5,327件の閲覧回数
golebiowski_bar
Contributor II

Hello,

This is my kernel version: 4.14.98-cl-som-imx7-6.3, so I'm using this datasheet for encrypt my data storage: AN12714 from 25 February 2020.

 

I have problem with keyctl. When I want to create secure key I get this communicate: add_key: No such device. What kind of driver I should install? I don't have these dependencies:

CONFIG_CRYPTO_DEV_FSL_CAAM_DESC=y

CONFIG_CRYPTO_DEV_FSL_CAAM_UTIL_BLACK_KEY=y

CONFIG_CRYPTO_DEV_FSL_CAAM_UTIL_BLOB=y

CONFIG_CRYPTO_DEV_FSL_CAAM_TK_API=y

CONFIG_CAAM_KEYS=y

in my kernel version. But I have similar ones:


# Random Number Generation
#
# CONFIG_CRYPTO_ANSI_CPRNG is not set
CONFIG_CRYPTO_DRBG_MENU=y
CONFIG_CRYPTO_DRBG_HMAC=y
# CONFIG_CRYPTO_DRBG_HASH is not set
# CONFIG_CRYPTO_DRBG_CTR is not set
CONFIG_CRYPTO_DRBG=y
CONFIG_CRYPTO_JITTERENTROPY=y
CONFIG_CRYPTO_USER_API=y
CONFIG_CRYPTO_USER_API_HASH=y
CONFIG_CRYPTO_USER_API_SKCIPHER=y
# CONFIG_CRYPTO_USER_API_RNG is not set
CONFIG_CRYPTO_USER_API_AEAD=y
CONFIG_CRYPTO_HW=y
# CONFIG_CRYPTO_DEV_HIFN_795X is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_COMMON=y
CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API_DESC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API_DESC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_KEYBLOB_API_DESC=y
CONFIG_CRYPTO_DEV_FSL_CAAM_SECVIO=y
CONFIG_CRYPTO_DEV_FSL_CAAM=y
# CONFIG_CRYPTO_DEV_FSL_CAAM_DEBUG is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_JR=y
CONFIG_CRYPTO_DEV_FSL_CAAM_RINGSIZE=9
# CONFIG_CRYPTO_DEV_FSL_CAAM_INTC is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_AHASH_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_PKC_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_API=y
CONFIG_CRYPTO_DEV_FSL_CAAM_TK_API=y
# CONFIG_CRYPTO_DEV_FSL_CAAM_TK_API_TEST is not set
# CONFIG_CRYPTO_DEV_FSL_CAAM_RNG_TEST is not set
CONFIG_CRYPTO_DEV_FSL_CAAM_SM=y
CONFIG_CRYPTO_DEV_FSL_CAAM_SM_SLOTSIZE=7
# CONFIG_CRYPTO_DEV_FSL_CAAM_SM_TEST is not set
# CONFIG_CRYPTO_DEV_SAHARA is not set
# CONFIG_CRYPTO_DEV_MXC_SCC is not set
# CONFIG_CRYPTO_DEV_MXS_DCP is not set
CONFIG_CRYPTO_DEV_VIRTIO=y
# CONFIG_ASYMMETRIC_KEY_TYPE is not set

Best regards

0 件の賞賛
返信
6 返答(返信)

5,306件の閲覧回数
golebiowski_bar
Contributor II

I enabled all dependencies and install all packages described in user guide. But still the same issue. Maybe this will help?

https://github.com/f-secure-foundry/caam-keyblob

0 件の賞賛
返信

5,264件の閲覧回数
Yuri
NXP Employee
NXP Employee

@golebiowski_bar 
Hello,

  Do You use Ubuntu 16.04 on the host?

Regards,
Yuri

0 件の賞賛
返信

5,246件の閲覧回数
golebiowski_bar
Contributor II
System:    Kernel: 5.4.0-26-generic x86_64 bits: 64 compiler: gcc v: 9.3.0 Desktop: Cinnamon 4.6.7 
           wm: muffin dm: LightDM Distro: Linux Mint 20 Ulyana base: Ubuntu 20.04 focal 

5,237件の閲覧回数
Yuri
NXP Employee
NXP Employee

@golebiowski_bar 
Hello,

  Could You try Ubuntu 16 ?

 

Regards,
Yuri.

0 件の賞賛
返信

5,229件の閲覧回数
golebiowski_bar
Contributor II

The problem is with missing driver, not with keyctl.

0 件の賞賛
返信

5,317件の閲覧回数
Yuri
NXP Employee
NXP Employee

@golebiowski_bar 
Hello,

 Use also  section 9.5 (Disk encryption acceleration)
of "IMX_LINUX_USERS_GUIDE.pdf"

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

Regards,
Yuri.

0 件の賞賛
返信