Encrypted RootFS using i.MX8MQ using yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Encrypted RootFS using i.MX8MQ using yocto

2,625 Views
harshitshah
Contributor III

Hi @marouene_boubakri ,

We have seen in one thread about the document over imx6q for encryption. 

Please provide access to the document "Root filesystem encryption using DM-Crypt" provided in this link. 

https://community.nxp.com/docs/DOC-342300

Please provide access to the above link so we can access all the commands properly. (Please send the access of this actual link and not the PDF version as some of the commands are cropped in that version.)

Regards.

0 Kudos
Reply
2 Replies

2,558 Views
harshitshah
Contributor III

Hi Igor,

 

Thank you for the reply. We reffered AN12714, however it is not providing all the details.

1) How to add support for encryption of rootfs?

2) What are the steps required to integrate the same to Yocto? 

 

Those steps are missing in AN12714. So we require the support for https://community.nxp.com/docs/DOC-342300.

Can you please check internally and provide the same?

 

Regards.

0 Kudos
Reply

2,603 Views
igorpadykov
NXP Employee
NXP Employee

Hi Harshit

 

that link is currently empty as its content was published in AN12714

i.MX Encrypted Storage Using CAAM Secure Keys

 

Best regards
igor