Encrypt the u-boot image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Encrypt the u-boot image

1,643 Views
vinothkumars
Senior Contributor IV

Dear NXP,

 

Platform: IMX8Mnano

OS: Yocto

 

Is there any configuration for the encrypt u-boot image ?

 

 

 

 

Regards,
Vinothkumar Sekar
0 Kudos
Reply
3 Replies

1,635 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Vinothkumars

 

You can see at the following link:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Encrypted-U-boot-Example/ta-p/1102981

 

Regards

 

0 Kudos
Reply

1,631 Views
vinothkumars
Senior Contributor IV

Thank you @Bio_TICFSL for the reply.

 

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Encrypted-U-boot-Example/ta-p/1102981

 

Above link used for iMX6 Solo X. But, I am looking for IMX8MNano.

Will you please provide to IMX8MN ?

 

 

Regards,
Vinothkumar Sekar
0 Kudos
Reply

1,626 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Vinothkumars,

 

We don´t have an example for the MX8, but the sample on MX6SX works for MX8 as well.

 

Regards

 

0 Kudos
Reply