Encrypt and Decrypt the EMMC partition in Yocto Source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Encrypt and Decrypt the EMMC partition in Yocto Source

2,326件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

 

Platform: IMX8MNano EVK

OS: Yocto

 

I needs to enable configuration in yocto source to encrypt and decrypt the EMMC partition.

I unable to find exact guide to encrypt and decrypt EMMC Partition in yocto source itself.

I have FitImage (Kernel, dtb, Initramfs). Is there way for encrpt and decrpt the boot partition from u-boot

source.

 

I need some document or expert help to proceed further. 

 

 

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,305件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

It is related to uboot and kernel config.

Here is commands:

bitbake linux-imx -c menuconfig

bitbake uboot-imx -c menuconfig

 

BR

Zhiming

 

0 件の賞賛
返信

2,300件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you @Zhiming_Liu for the quick reply.

 

Is it possible to add encrypted partition in .wic (.wks) file ?

Regards,
Vinothkumar Sekar
0 件の賞賛
返信