Encoder capacity and video input solution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Encoder capacity and video input solution

Jump to solution
1,687 Views
kevinatnxp
Contributor I

Hi there,

We are looking for a new platform from Nvidia Jetson. And have couple questions.

1. I checked the specs that none of the imx8 series support encoding H.265/H.264 at 4K level, is this true? Is the 1080p the maximum encoder resolution it can support?

2. I noticed that imx8 have HDMI input hardware available for video input. But there are no documents talking about this, My question is when will this be available, and what is the specs(HDMI2.0)?

Thanks 

Kevin

0 Kudos
Reply
1 Solution
1,680 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

 

1. video capabilities are described on link:

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

2. right, it is HDMI 2.0, regarding future plans, such  details can be provided in local marketing office.

 

Best regards
igor

 

 

View solution in original post

0 Kudos
Reply
1 Reply
1,681 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

 

1. video capabilities are described on link:

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

2. right, it is HDMI 2.0, regarding future plans, such  details can be provided in local marketing office.

 

Best regards
igor

 

 

0 Kudos
Reply