Enabling the FIELD_RETURN_LOCK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enabling the FIELD_RETURN_LOCK

1,445 次查看
nemik
Contributor I

Hello,

I am trying to enable the FIELD_RETURN_LOCK bit in OCOTP_SW_STICKY register on my "closed" (fused) imx7dsabresd board. 

I verified that I can only unlock OCOTP features by flashing the bootloader to NAND, otherwise it does not work in SDP mode over USB. I verified this by enabling the SRK REVOKE which did work when flashed, but not over SDP.

However nothing I try seems to let me enable the FIELD_RETURN_LOCK bit as described here: https://community.nxp.com/t5/Known-Limitations-and-Guidelines/Field-Return-dependency-on-OCOTP-Modul... also not sure why I can't access that document now, but could a couple of weeks ago. There is a cached version here: https://webcache.googleusercontent.com/search?q=cache:kkLTvDfCjUsJ:https://community.nxp.com/t5/Know...

I test the OCOTP_SW_STICKY using "md 0x303500B0 1" in U-Boot and always get 0x18 and did manage to get 0x1C when enabling SRK Revoke, but it did not enable FIELD_RETURN.

My board's UID is "000001266e48126a" and I see this running

$ cat /sys/fsl_otp/HW_OCOTP_TESTER0 
0x6e48126a
$ cat /sys/fsl_otp/HW_OCOTP_TESTER1
0x126


and also when printing it from U-Boot using the tag_serialnr struct.

In my CSF file, I am adding:

[Unlock]
Engine = OCOTP
Features = FIELD RETURN, SRK REVOKE
UID = 0x00, 0x00, 0x26, 0x01, 0x48, 0x6e, 0x6a, 0x12

and different combinations of the UID but can't seem to turn off the FIELD_RETURN sticky bit.

Any help is appreciated. Thank you,

Nemanja Stefanović

0 项奖励
回复
1 回复

1,437 次查看
Yuri
NXP Employee
NXP Employee

@nemik 
Hello,

  I've sent You some comments directly.

Regards,
Yuri.

0 项奖励
回复