Hi,
I am trying to enable Parallel Camera interface on iMX6QDL-VAR-DT6 Custom board. I am using e-CAM51_CU5640_MOD OV5640 Camera module and is connected to the VAR-DT6 custom board J11 parallel camera interface via a custom interface board. As per the VAR DT6 Custom board documentation, this is directly connected to the IPU2 CSI 1 interface of the IMX6 processor. Accordingly I have made the following changes in the Linux Source code (Version 3.14.38-6QP) (The yocto release version information is VAR-SOM-MX6 - Yocto fsl-3.14.38_6qp Fido R2 Build Yocto release)
1. mach-imx6q.c
static void __init imx6q_csi_mux_init(void)
{
.....
else if (of_machine_is_compatible("fsl,imx6dl-sabresd") ||
of_machine_is_compatible("fsl,imx6dl-sabreauto"))
regmap_update_bits(gpr, IOMUXC_GPR13, 0x3F, 0x0C);
else if (of_machine_is_compatible("fsl,imx6q-var-dart"))
{
regmap_update_bits(gpr, IOMUXC_GPR1, 1 << 20, 1 << 20);
}
....
}
2. imx6qdl-var-dart.dtsi
v4l2_cap_1 {
compatible = "fsl,imx6q-v4l2-capture";
ipu_id = <1>;
csi_id = <1>;
mclk_source = <0>;
status = "okay";
};
ov5640: ov564x@3c {
compatible = "ovti,ov564x";
reg = <0x3c>;
clocks = <&clks 201>;
clock-names = "csi_mclk";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu1_2>;
pwn-gpios = <&gpio3 3 1>;
rst-gpios = <&gpio3 10 0>;
csi_id = <1>;
mclk = <24000000>;
mclk_source = <0>;
};
pinctrl_ipu1_2: ipu1grp-2 { /* parallel camera */
fsl,pins = <
 MX6QDL_PAD_EIM_D28__IPU2_CSI1_DATA12 0x0001B0B0
MX6QDL_PAD_EIM_D27__IPU2_CSI1_DATA13 0x0001B0B0
MX6QDL_PAD_EIM_D26__IPU2_CSI1_DATA14 0x0001B0B0
MX6QDL_PAD_EIM_D20__IPU2_CSI1_DATA15 0x0001B0B0
MX6QDL_PAD_EIM_D19__IPU2_CSI1_DATA16 0x0001B0B0
MX6QDL_PAD_EIM_D18__IPU2_CSI1_DATA17 0x0001B0B0
MX6QDL_PAD_EIM_D16__IPU2_CSI1_DATA18 0x0001B0B0
MX6QDL_PAD_EIM_A24__IPU2_CSI1_DATA19 0x0001B0B0
MX6QDL_PAD_EIM_D23__IPU2_CSI1_DATA_EN 0x0001B0B1
MX6QDL_PAD_EIM_D17__IPU2_CSI1_PIXCLK 0x0001B0B0
MX6QDL_PAD_EIM_DA11__IPU2_CSI1_HSYNC 0x0000B0B1
MX6QDL_PAD_EIM_DA12__IPU2_CSI1_VSYNC 0x0000B0B1
>;
};
When I run the gstreamer application against video1 device,
gst-launch imxv4l2src device=/dev/video1 ! imxv4l2sink
the application hangs waiting for the camera_callback and times out with the de_queue error message.
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
rc0: Internal data flow error.
Looking forward for some pointers to resolve this issue.
Thanks,
Prashanth
I had a similar problem try to interface an ov5642 camera to the iMX6QDL-VAR-DT6 Custom board. I eventually got it to work, but had to delete the mipi camera from the device tree.
I can see some mistakes in the pin muxing, in particular:
      MX6QDL_PAD_EIM_A16__IPU2_CSI1_PIXCLK 0x0000b0b1
needs to be correct. 
I have DATA_EN pulled high, and pick up CLKO2 from J17.3 (a 33R in series seems to help with signal integrity).
Curiously, if I add the mipi camera stuff back in, the mipi camera works on /dev/video1, but the ov5642 stops working on /dev/video0 (mxc_v4l2_capture.out gives:
"Unable to open /dev/video0")
Hi Prashanth
one can try to use patch "0001-IPU-update-IPU-capture-driver-to-support-up-to-four-.patch" to
support camera on any IPU's CSI port.
https://community.freescale.com/docs/DOC-158531
https://community.freescale.com/thread/330749#435854
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for your quick reply. The base version of the patch file is different from the one I am currently working on. I will look into the patch file and try to manually modify my code base.
Meanwhile I was looking for some short work flow to make my parallel camera stream video to the HDMI output. I am not worried about the MIPI interface at the moment. I just need the video input from my parallel camera (connected to J11 jumper of VAR DT6 custom board) to be displayed onto the Monitor (640 x 480) via HDMI interface. Is there any such documentation or sample code that I can refer to ?
Thanks,
Prashanth