Enabling PWM in IMX93EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling PWM in IMX93EVK

1,623 Views
Robbi
Contributor III

Hi team,

                  I am try to blink led on IMX93EVK using PWM based on document provided by NXP.

  1.   They had provided 2 dts files :
    imx93-11x11-evk-pwm-led.dts
    imx93-11x11-evk-pwm.dts
  2. I copied these 2 files in u-boot-imx/git directory.
  3. And changed
    CONFIG_DEFAULT_DEVICE_TREE="imx93-11x11-evk-pwm-led" , 
    CONFIG_DEFAULT_FDT_FILE="imx93-11x11-evk-pwm-led.dtb"
    imx93_11x11evk_defconfig file.
  4. Added 
    dtb-$(CONFIG_ARCH_IMX9) +=imx93-11x11-evk-pwm-led.dtb in Makefile.
  5. Final performed build, but there is no change in the image.

Please guide me the steps to test below PDF and steps to configure dts file.

How/where  to add below two files and because I am seeing work/work-shared directory.

 

 

 

Thanks Robbi.

0 Kudos
Reply
1 Reply

1,599 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Robbi!

Thank you for contacting NXP Support!

 

The device tree files should be applied in Linux Kernel not in u-boot device tree.

You can compile the device tree file using this guide.

 

Best Regards!

Chavira

0 Kudos
Reply