Enabling LCD display in i.MX50 EVK with Linux release -blog archive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling LCD display in i.MX50 EVK with Linux release -blog archive

1,150件の閲覧回数
GraceH
Senior Contributor II

In Linux BSP, by default, the LCD framebuffer is not enabled.  SEIKO and CLAA driver are also disabled.

The kernel need be re-configure to enable LCD framebuffer.

In kernel configuration menu, go to device drivers -> Graphics Support

Select "SEIKO WVGA Panel"

Select "CLAA WVGA Panel"

Deselect "E-ink Panel Framebuffer"

Select "Support MXC ELCDIF framebuffer"

Then in command line:

 

1. with SEIKO LCD (connected on J13)

setenv bootargs_mmc 'setenv bootargs ${bootargs} console=ttymxc0 root=/dev/mmcblk0p2 rootwait rw lcd=1'

2. with SEIKO LCD (connected on J12)

setenv bootargs_mmc 'setenv bootargs ${bootargs} console=ttymxc0 root=/dev/mmcblk0p2 rootwait rw lcd=1,j12'

2. with CLAA LCD

setenv bootargs_mmc 'setenv bootargs ${bootargs} console=ttymxc0 root=/dev/mmcblk0p2 rootwait rw lcd=2'

タグ(1)
0 件の賞賛
返信
0 返答(返信)